Hi Sir,
I can find Over current and Over temperature Protection features in TPS75105 datasheet.
Can you have more detail about these features?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Frank,
For the overcurrent protection, the internal current source will sense the output current and when it will trigger OCP protection when the output current is over 35mA;
For over-temperature protection, it will shutdown when it triggered the over-temperature point.
BR
Sean