This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/UCD3138: Regarding 16 bit PWM Timer

Part Number: UCD3138

Tool/software: Code Composer Studio

I use a UCD3138RGC(64pin).
I use the following address code.
www.ti.com/.../UCD3138FW-PSFB (UCD3138 Phase Shift Full Bridge Firmware)
The following is described in Section 11.12 of the Technical Reference manual.
"The C code below should provide an approximate 10 KHz interrupt from the T16:
TimerRegs.T16PWM0CMP0DAT.bit.CMP_DAT = 1587; //value to reset counter "
Please tell me the frequency of T16 counter.