Hello TI,
Currently we are using BQ24773 Battery charging IC,
1. BQ24773 support Parallel battery cell connection if yes, what is maximum capacity of Battery pack & battery pack capacity support ..?
2. BQ24773 what is the ideal condition & requirement of Parallel battery pack connection configuration..?
3. We are planning to use Lithium Ion INR21700 M50 18.20Wh(LGM50) , Connecting 4 cell parallel to achieve required battery capacity to our system, there is any recommendation for that or is it suitable to BQ24773 ..?
4. As per the design requirement Bq24773 is suitable..? if there is any better replacement of BqQ4773 please suggest us.
Thanks,
Rahul