We have a Lithium-Ion Smart Battery application that is a 4 series with 50 batteries in parallel for each group in series. The continuous charge current is 82.5 A and the continuous discharge current is 125 A. Please recommend a gauge IC.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have a Lithium-Ion Smart Battery application that is a 4 series with 50 batteries in parallel for each group in series. The continuous charge current is 82.5 A and the continuous discharge current is 125 A. Please recommend a gauge IC.
Hello David,
I would recommend using the top of stack gauge bq34z100-g1 if you only need a gauging solution. If you need more functionality, you can look into the bq40z50 or bq40z80 for protections/cell balancing, but the discharge current may be too high for them to scale.
Sincerely,
Wyatt Keller