This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCPA10512: Isolated Low-power Capacitively-Coupled Supply (Low EMI)

Part Number: DCPA10512

Hi Guys,

I'm designing a low-power isolated supply (3.3V, Max ~50mA) and am keen to steer clear of transformers as EMI is critical to the design and I've had some noise issues with my previous transformer-based design.

I have been looking at using a capacitively-coupled circuit plus bridge rectifier as per Maxim's AN4553 app note - see below  (or a similar charge-pump type circuit which will allow me to get ~150mW of power across the isolation caps) but their MAX256 chip is far overspec'd from a power (and size/cost) point of view (3W) for my requirements.

Do you have any suggestions for a driver to replace the max256 here, which would differentially drive a square wave into a circuit like this at <2 MHz? Or is there an alternative way to achieve a capacitively coupled low power supply? I've had a look at some cmos drivers, even 555 timers, but nothing seems to provide the combination of (a) required source/sink output power and (b) dual, complimentary square wave output I require to drive into the capacitor/bridge circuit.

Since it is such a low power application, am hoping there is a cheap, small, quiet way to do this easily, but so far I haven't found it.

Thanks in advance, 
Dave