Other Parts Discussed in Thread: UCC28730, UCC28910
Dear TI Team
Our customers are looking for reference designs and devices that meet the following conditions:
・ AC85 ~ 264V input
・ 5V 0.5A output
・ Non-insulated type
I searched for a reference design, but there is no design that can output 2.5W (5V, 0.5A), and there are only designs with output up to 2W (20V, 0.1A) as shown below. (I checked on WEBENCH, but only the Flaback configuration appears.)
https://www.ti.com/tool/PMP4443
https://www.ti.com/tool/PMP20834
Please let us know if there is a reference design or solution that meets the above conditions.
Best Regards,
Y.Ottey