Other Parts Discussed in Thread: PMP20196
Hi
The customer asked the schematic PMP20196, is it recommended to use it under the following conditions?
Power range isolation: 18~75V
Output voltage: 5V @ 4A~5A, OCP:> 7A
61850-3 >>> 500~1KV, 500V (minimum requirement)