This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS709-Q1: Exact replacement for AP7370-50W5-7

Part Number: TPS709-Q1
Other Parts Discussed in Thread: TPS709, TPS7B69, TPS7B69-Q1

Hello Guys,

Good day.

Our customer's PCB design have already been done and mass-produced, but they are having shortage of  AP7370-50W5-7 and is looking to TPS70950QDBVRQ1 as an exact replacement in footprint, pinouts and functionality. Their minimum functional requirements are the following:

* Output voltage = Fixed - 5.0 V

* Output voltage tolerance: 3% or better

* Input voltage max > 17 V

* Output current max >= 150 mA

Would TPS70950QDBVRQ1 be a good fit? They are open for any suggestions. Below is the link to the device datasheet.

www.diodes.com/.../AP7370.pdf

Thanks!

Art