Other Parts Discussed in Thread: TPSM5D1806, TPS543620
Hello,
I'm using the TPS53015 device as a step-down converter to generate 5V out of a battery. I would like to guarantee that the device will not be damaged or will not generate a different tension than 5V when VIN gets too low.
0/ Can the device be damaged or VOUT falls below 5V when VIN gets too low?
1/ Does the device disable itself without any external circuitry if VIN gets too low for the required VOUT (=5V) ? I'm a bit confused what the UVLO protection is in the datasheet and what its purpose is.
2/ Is there a way to disable the device when VIN goes below a specific voltage (around 8 V) ?