This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: With out BAT, Vsys not output power

Part Number: BQ25703A


Hi ,

Without BAT( CELL_BATPRES:0 V), Vsys connect to backup battery

The system supply by batteryup battery, and insert Input power source(19V or 15V)。 The Vsys will drop and power on again. What reason leading the issue?

And I use BQ25703AEVM to debug, if set to no BAT, inset power source(without wirte I2C register ), Vsys no output power.

If set to 2cell, inset power source(without wirte I2C register ), Vsys output 6.12V.

Is it because the I2C register was written in the wrong time?And other reason?