Following the sequence mentioned in your Example code we are unable to load to SRAM that we are running on a custom board(MCU MSP432)
- Can anyone list the sequence of register write to load program and enable the engine after loading program
- If i2c auto increment is enabled can we write in one byte mode(start -- finish) (start -- finish)
- How should you write the program memory in one byte mode or two byte mode (start -- next data - next data -- ... ... -finish)
- Can we program load custom board using your GUI interface