When operating at room temperature at 22°C to our high temperature at 71°C, the converter operates as designed. When the chip is brought down to -40°C, the output voltage seems to be bucking down to 13.1V. I monitored the high-side driver and low-side drivers and can confirm that the chip is operating in the buck region, rather than the buck-boost region we see at room temp. The reference voltage for the feedback is set to 0.8V, and the feedback we are seeing is 0.67V. This is what is expected with our resistor divider. Measuring the soft-start pin we see the voltage at 1.2V as expected and the comp pin is railed high at 3.2V as expected. With these conditions, the converter should provide some boosting in order to get the voltage up. I can confirm that PGOOD is low. Since I have control on the input voltage, I see that lowering the input voltage causes the converter to stay in buck and lowers the output voltage. Increasing the output voltage I can get to my 15.75V output once the input voltage reaches 19V. As I raise my voltage above that, the converter regulates the output at 15.75V (showing that the error amplifier is operation and that the Vref is still set to 0.8V with tolerances).
For some background:
Input Voltage: 15.8V
Output Voltage 15.75V
Output Current: 1A
Operating Temperatures: -40°C ambient to 71°C ambient