This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Part Recommendation Inquiry

Hi, TI expert.

The customer requested a part recommendation that meets the specifications and conditions below.

--------------------------------------------------------------------------------------
1) Input: 3-phase 4-wire single-phase standard (220V +-20%)

2) Output: 4 channels
- DC 12V, 30W
- DC 12V, 12W
- DC 12V, 12W
- DC 12V, 12W

3) Requirements
a) Input, output isolation, output 4-channel GND separation
b) Each output power overcurrent protection
c) Regulation output voltage within 3%
d) Products capable of initial IC operating voltage DC
e) IC with input control (enable pin)
f) Total efficiency over 81%
g) Operating temperature -25 degrees to 70 degrees
--------------------------------------------------------------------------------------

Are there any recommended parts?

please answer about my question.