Good Morning
I would like to power a system from SYS pin.
How can i force the "unknown power adapter" status in the circuit?
Also i noticed that if i draw more than 0.2A (is the start-up input current limit) from SYS and battery isn't present the circuit shut down and restart (loop)---> Is anything i can do to forse the circuit as "buck regulator" without battery?
I would like to use it as main power supply even if battery isn't good. But i'm unable to force it to ILIM status (380Ohm) and it shut-downs every time i draw too much current on start without battery.
Thanks