Hi Team,
we plan to use the attached 15uH Wuerth transformer out of the WE-MAIA series in combination with LMR36503-Q1. Vin 9-16V, Vout 5V, Iout max 150mA. The DCR is higher than what we recommend in the datasheet, on the other hand we only need 150mA max. Do you have experience with these transformers in combination with the LMR36503-Q1? Do you see any concerns?
78438335150_valid_from_2021-01-30.pdfmany thanks Lutz