Other Parts Discussed in Thread: BQ24765
Hello,
We are using BQ24765EVM with a battery. We are facing an issue while charging the battery. Battery is requesting charging current 3000mA and charging voltage 12300mV. We are writing the requested current and voltage in BQ24765EVM. Battery starts charging for two minutes. We have confirmed this by reading supplied current in battery (and also battery percentage/capacity increased a little bit). But, after two minutes, battery is reporting supplied current is 0mA (gradually decreases from set current) and and there is no error in battery status. We have checked the set charging voltage and charging current in BQ24765EVM and it is same as set value. No clue, why it stops charge after some time... If we write again the charge current and voltage to BQ24765EVM, then battery starts charging for some time and stops.... can you help to fix this issue?
Thanks and Regards,
Elavarasan