Hello. Formula 22 in the LM46002 data sheet is yielding results that do not make sense. I am getting values much larger than expected. Can someone check this formula? It looks like there is a typo there.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello. Formula 22 in the LM46002 data sheet is yielding results that do not make sense. I am getting values much larger than expected. Can someone check this formula? It looks like there is a typo there.
Hi Charles,
I believe the equation is correct for Cff. I calculated the application example in the datasheet and came up with the correct value. Make sure you are using the value for fx in kHz and calculating the parallel value for Rfbt//Rfbb correctly.
What values are you using for fx, Rfbt and Rfbb?
Also, look at Table 2 of the datasheet for recommended values.
It looks like you tried posting an image in you post, but it didn't show up. Not sure what you were trying to post.
Regards, Jason
Also, the parameter for voltage undershoot is not given in the design example, as far as I can see. What is the value for the example?
Hi Jason,
For the design example given with Vout =3.3V and 47uF X 3 capacitors, I get fx=0.009348 (using 141uF. If I use capacitance in Farads, it is 9348. Is that what you get?
Next, for Cff calculation I am not getting anything like 47pF. Would you be able to write out the detail of the calculations?
Hi Charles,
Yes, that's what I get for fx. Sorry, I said uF, but I meant F.
For Cff = 1/(2*pi*9348) x 1/√(1000000*303000) = 30.1pF
I know it's not 47pF, but it gives you a result in the tens of pF.
They probably used the value shown in table 2 for selecting typical components.