Hello again;
For some reason the "Ask a related questions" button isn't working for me, so I'm submitting a new issue, but involving the same calibration question.
It appears that I cannot write to the CC Offset RAM manually? It seems that the gauge won't allow me to do so. I enter calibration mode as per the TRM, collect 8 samples using the Analog Conversion Counter, average the samples, and then attempt to write the Gauge with the new CC Offset value...But it won't take.
Will you please confirm that this gauge will only update the offsets by issuing the BOARD_OFFSET: 0x0009 and/or CC_OFFSET: 0x000A command(s), followed by the CC_OFFSET_SAVE: 0x000B command?
If so, it's very disappointing, since it takes forever.
Thanks