Hi Team,
On the LM2755 datasheet we mention that the shutdown supply current of 5uA typ can be achieved when EN1 = EN2 = EN3 = 0. Does HWEN accomplish this as well as Bits 0,1,2 in the General purpose register (0x10)?
Thank you,
Jon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
On the LM2755 datasheet we mention that the shutdown supply current of 5uA typ can be achieved when EN1 = EN2 = EN3 = 0. Does HWEN accomplish this as well as Bits 0,1,2 in the General purpose register (0x10)?
Thank you,
Jon
Hi Jon,
please reference to the Figure 10 in the datasheet. Shutdown current is test when EN1=EN2=EN3=0 and HWEN=VIN. When the HWEN is driven low, all internal control registers reset to default states include BIT0,1,2 in the general purpose register to be '0'. Only pull down the HWEN and pull it up to Vin can we enter the shutdown states.
Best Regard
Monet Xu