This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54308: TPS54308 Directly replace TPS54302

Part Number: TPS54308
Other Parts Discussed in Thread: TPS54302,

Hi team,

Customer originally using TPS54302 in their DVR application, with 12V input and 5V output, 10uH inductor, with SCH as below.

Recently they want to replace TPS54302 with TPS54308, is that possible to directly replace without any SCH changing?