Other Parts Discussed in Thread: CSD25404Q3, CSD16570Q5B, CSD17570Q5B, CSD17581Q5A
Hi Team,
I am designing a battery-operated system whose input charging current is about 10A maximum and the discharge current is up to 40A maximum.
The 40A current will only last for a few minutes(10 minutes maximum) but all the other time the expected current is 10-15A(1-hour maximum).
I'll need both P-channel as well as N-channel MOSFET in my application.
The CSD25402Q3A has a maximum current of 76A.
But how a small device like this can handle such a high current without damaging itself?.
My required drain voltage is 12.8V
Also, how can I design a thermal heatsink to transfer heat effectively for such SMD components?.