Part Number: LM61460
Hi team,
I received a question about the inductor selection from my customer.
The d/s states that "The saturation current rating of the inductor must be at least as large as the high-side switch current limit, IL-HS". Therefore, I think customer needs to choose an inductor with a saturation current of at least 11.5A if the duty cycle is less than 35% from Fig.19. I think the definition of saturation current varies among inductor manufacturers. Is it correct that saturation current is <30% from normal inductance value? It seems that the EVM employs Wurth's 74439346047 which rated current is 7.4A and Isat is 14.7A(<30%).
Customer's condition
Vin=24V, Vout=3.3V, Iout=4.5A. L=3.3uH.
Customer cannot use large size inductor due to space limitation. However, when they try to meet 11.5A to support short circuit protection, the inductor size becomes larger.
Regards,
Yamaguchi