This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5088: -48V output not regulating and seems to be stuck resetting /hiccup mode (LM5088-2)

Part Number: LM5088
Other Parts Discussed in Thread: LM5118, LM5085

I am having an similar issues but have +20V regulated in and trying to get -48V out for POE application.

I add some caps from Vin to -Vout (2.2uf|| 0.1uf) as suggested but having issues it is not regulating but only get ~-20Vout.

The system seems to be current limiting and reset/hiccup at ~100Hz. 

Vref is only getting to ~0.46V, so not regulating, switching freq set at ~550kHz, 10uH 6.9mohm ind,

I used Webench design setup and the TI excel calculator (+75Vin +48Vout) to derive the compensation values.

What am I missing? it is acting like the system is over current and resetting/hiccup mode, the output is current at no load.