i am using BQ76930 with 8 cells . I connected my circuit to the power supply and every thing was ok. then i connected circuit to the inverter/charger (Victron multiples ii) then I saw cell num4 voltage goes up and down between 3.5 to 4.1 volt. all others cells working correctly just problem with cell4 value. I got cell num 4 voltage by multimeter and it was 3.76
i checked it again with power supply and cell 4 worked correctly . so cell number 4 value changing when i am using inverter/charger .it is very important for me to use this project by inverter/charger because i want to use it as home storage .
i also change capacitor and resistor according to the slua810 Figure 4 but it didn't worked .
r356 connected via wire in battery pack.