This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Please help recommend the charging management chip

Other Parts Discussed in Thread: BQ25713, BQ24610

Dears

Please help recommend the charging management chip:

1. Lithium ion battery cell, 4PCS, 32700/6000mAh, lithium iron phosphate;

2. The maximum charging current is 6A;

3. Support battery thermistor temperature detection;

4. Industrial grade;

Thanks

Elsa Duan

  • Hi Elsa,

    If you have a host processor with I2C and can write software, I recommend BQ25713.

    If you do not have a host processor and have a input power source > final battery voltage, then I recommend BQ24610.

    Regards,

    Jeff