Other Parts Discussed in Thread: LMZ14203,
Hello TI support,
the package of the TPS92551 is similar to some other products like LMZ14203 and others. The storage temperature of TPS92551 is 0°C to 150°C and the LMZ14203 is -65°C to 150°C.
Does this mean that TPS92551 is not allowd to be stored and to operate below 0°C. I think about a pocket light for outside temperatures when it snows.
Is there a legal binding statement for temperatures below 0°C ? Do you know the reason why it is 0°C, because IC, R,C and L should have no problems with -65°C.
Best regards,
Roland