This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCPA10515D: Confirmation Topology

Genius 9880 points
Part Number: DCPA10515D


Hi Team,

Good day, we received a query from customer and for me to not miss any information, I'll copy the query below.

"

I'm looking for a small volume DC DC converter (<5W) with input voltage <7V and output voltage of approximately 3V.
I'm trying to evaluate the DCPA10515D and UCC12050 but could not find the topology which makes it harder for me to choose. Is it a resonant topology like LLC or flyback? I don't need specific implementation details but it would help if you can comment of the topology of the power stage.

"

Thank you and looking forward for your kind response.

Regards,

Maynard

  • Hi Maynard,

    The DCPA1 devices use a monolithic push-pull driver.

    DCPA1 devices only operate from 5V input and offer ±5, ±12, and ±15V output options.

    The DCP01 & DCP02 devices are also push-pull but offer more VIN and VOUT options.

    Regards, Jason