This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Device recommendation request.

Other Parts Discussed in Thread: UCC28061

Hi, TI expert.

We request a device recommendation that meets the specifications and conditions below.

--------------------------------------------------------------------------------------------------------
- Input: 3-phase 4-wire single-phase standard (176Vac~264Vac)

- Output: DC 12V, 30W

- Requirements
1) Input, output isolation
2) output power overcurrent protection
3) Regulation output voltage within 3%
4) Products capable of initial IC operating voltage DC
5) IC with input control (enable pin)
6) Total efficiency over 81%
--------------------------------------------------------------------------------------

We request a device recommendation that meets the above conditions.

Thank you.