Hi,
I made a PCB where are used to boost 2.8V to 5V 1A out, however it is not working properly.
I tested it by providing analog voltage from my laboratory PSU 2V - 4V. The output is always the same, just passing the input voltage to the output, never 5V. In more details if I provide 2V the output is 2V, if provide 3V the output is 3V etc.
I check the schematic 1000 times, also the PCB, looks OK to me.
Can you please check them and comment.
Thank you in advance.
Kind Regards
Ioannis