This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: bq28z610 accuracy

Part Number: BQ28Z610
Other Parts Discussed in Thread: GPCCHEM

Hi Expert,

The customer is using bq28z610 on the battery project.

The previous battery rating voltage they using is 4.35V. while the battery is EOL, so they plan to use new batteries. The rating voltage of the new battery they selected is 4.4V. During the new battery evaluation, the customer use the same chemical ID as before. when the battery goes to a pretty low level, like 3% or 5%, it will go to 0% directly. This phenomenon can be found in room temp and high temp condition.

The customer would like to know why it will drop from 3% or 5% directly to 0%. Is it caused by the different battery that the customer using?