The ADC equivalent input resistance in the data sheet shows 2.5k ohm max, which means it could even be lower. We intend to drive the ADC inputs with either direct regulator voltage outputs, or with op-amp buffering from dividers. But the data sheet also recommends a 200 ohm series resistor into the ADC input. With a 2.5k ohm equivalent input resistance, and a series 200 ohm input resistance, doesn't that create a large analog error in the ADC reading? What is the variation or range of the equivalent input resistance?