This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65381A-Q1: Is there a way to access internal error signals without using DIAG_OUT pin?

Part Number: TPS65381A-Q1

Hello Power Management Support-Team,

I have question regarding the function of the  DIAG_OUT pin. Table 5-5 to 5-8 list the internal error signals that are accessible over the DIAG_OUT pin. If I understand correctly a certain signal can be read from the DIAG_OUT pin after sending the appropriat command over SPI.

(Q1) Is it possible to access the the digital error signals from Table 5-5 to 5-8 by SPI, when the DIAG_OUT pin is not used?

Thank you and best regards,

Max