Other Parts Discussed in Thread: TPS2121
Dear Sir or Madam,
my question regards to set two TPS2113A in parallel to get a higher current delivery. Unfortunately I cannot find an alternative switch with the same conditions but with a higher current of approx. ~3.5A.
I want to use the VSNS comparator to decide the switching process through different input voltage levels. But if two switches are working parallel there are two comparators which has to be feed with one resistor divider. I guess through the tolerances the switching process will not work synchron. Correct?
Do you have some experiences to interconnect parallel two TPS2113A with a optimal synchronisation? Can you give some advices/recommendations?
Of course I am open for an alternative switch but I cannot find an identical one with a higher current delivery.
Thank you very much beforehand.
Best regards
Wolfgang Walter