Hi team,
I plan to pull up MODE pin to set Auto mode.
Should I pull it up to VOUT (3.3V use case) or VCC?
Is there any concern if I pull up either of the supplies?
*MODE pin is connected to VCC on top of the datasheet simplified schematic.
I concern about the description in the datasheet as below
1. VCC should not be loaded externally,
2. Don't float MODE pin.
regards,