This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3808: can we enlarge Propagation delay time

Part Number: TPS3808
Other Parts Discussed in Thread: TPS3899

Hi

I want to MR# low and "wait 1s" then reset# change high to low.

is possible ? 

and any material is suitable ?

  • Hi Dimitry,

    We cannot edit the prop delay on the TPS3808.

    We do have an alternate device that can help. The TPS3899 has a sense pin that has a programmable "sense delay" which can be increased to 1s before reset goes from high to low. Would this work?