This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61093: TPS61093 without discharge function.

Part Number: TPS61093

Hi,

My customer does not required discharge function.
What device is recommend with TPS61093 without discharge function?  Please advise us.

His requirement spec is as follows:

  • Vin 1.5V-3V
  • Vout 12V
  • Current Min 100mA
  • No need discharge function.

Please advise us.

Thanks and best regards,
M.HATTORI.