This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62808: 2.2uH design

Part Number: TPS62808

hi,

is there any data or expectation while using 2.2uH as inductor?

I know we recommend 1uH max, just wondering if that has ever been tested.

thansk a lot 

KR

Vincenzo

  • Hi Vincenzo,

    The device has been tested and characterized on bench only upto 1uH inductor and that is recommended in the d/s. Infact, the max values are as below.

    If the customer wants to use any value outside of the recommendations, it will be the customer's responsibility to confirm stability with their BOM. In any case, I would strongly recommend to follow the d/s recommendations.

    Please hit "Resolved" if you do not have any further questions.

    Regards,

    Febin

  • Hi,

    Let me attach the screenshot again.

    Regards,

    Febin