Part Number: BQ77915
Hi,
We have checked all protections again and again, all individually protections(testing 1 protection at once) are working good, but when say device is in OTC(Over Temp. during Charge) protection that Closes charging MOSFET gate, charging stops. After charger removal,if we connect Load and start Discharging(when device is in OTC protection) at high Currents above OCD, then Device doesn't go under protection and fails to turn off MOSFETS, & that results in Mosfet Burnout.
We have also noticed same problem when OCC protection is present and Load is connected then device not going under OCD protection & results in burnout of MOSFETS. Please provide Solution of this as soon as possible.
Device:; BQ7791501 under 10S configuration
LD resistance: 470k
Rsns:2mOhm
We have faced this issue after starting Production & production also hauled due to this Problem.
Please provide Solution asap.
Regards