This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610-R1: How to register the 'New chemistry id' of new battery?

Part Number: BQ28Z610-R1

I want to 'New chemistry id' of new battery.


How do I create a 'NEW CEHM ID'?

I send you my battery spec.

 ㅡ  TOOL  :  BQ-Studio

 ㅡ  Fuel Gauge  :  BQ28Z610-R1

 ㅡ  CELL Structure  :  2S-1P

 ㅡ  CELL MAKER  :  LISHEN

 ㅡ  CELL MODEL NO  :  SP454292SF  /  2910 mAh

 ㅡ  CELL Description  :  Rechargeable Lithium-ion Polymer Cell

 ㅡ  CELL Minimum Capacity  :  2910 mAh

 ㅡ  CELL Charging Voltage  :  4.4 V

 ㅡ  CELL Norminal Voltage  :  3.85 V  (0.2C Discharge)

 ㅡ  CELL Standard DisCharge Current  :  0.2 C   (582 mA)

 ㅡ  CELL Standard DisCharge END Voltage  :  3.0 V

 ㅡ  CELL Max Charge Current  :  1C  (2910 mA)

 ㅡ  CELL Max DisCharge Current  :  1C  (2910 mA) ㅡ 


Refer attached document for details.

GAC_LSN_SP454292SF CELL_승인원_201214.pdf