This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ79606A-Q1: BQ79606A-Q1 24 series lithium battery connection

Part Number: BQ79606A-Q1

HI

    Item: 24 strings BMS using 4PCS BQ79606

For example, if only No. 1 or No. 2 terminal is inserted, the BQ79606 part will be powered on. Is there any hidden danger in this way?

  • Hi User,

    So I think you are referring to "hotplug" event or random cell connection correct? The bq79606a datasheet explains it was designed for hotplug events if our recommended application circuit was followed correctly. However, when possible it is best practice to connect lower voltage cells first and then continue in upwards order.

    Regards,

    Taylor