Hi
Customer test has a problem
Waveform. Light load (0A) at 12.5V~12.7V to 12V
Why does the entire voltage float?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Gareth,
To me this looks like normal regulation behavior as the device is in the middle of buck-boost operation, noise on the board can easily get it from buck into boost mode or vice versa. The ripple is still within a range that I think is ok.