Other Parts Discussed in Thread: TPS5420,
Hi Team,
Need your inputs on our customer's query. They're working with the TPS5450 in a 12V input, 5V output condition. Problem is that the converter does not disable upon pulling ENA pin to ground. 2V output voltage is continuously being measured using the scope probe. There is no inductive or capacitive load in the circuit. The 5V generated by the TPS5420 is the only power source in the circuit so there is no back-power issue or leakage that may contribute to the issue. Can you help us on other possible root cause?
Attached is the schematic for reference. Thanks in advance!
Kind Regards,
Jejomar
x1.pdf