This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24770: About recovery operation from WDT

Part Number: BQ24770


Hi,

There is a problem that the system voltage fluctuation is large when returning from WTD.
Is it possible to suppress the voltage rise by changing the settings?
Please tell me how to make the recovery from the WDT reset operation a soft start.

Vin:24V
Battery : 3cell Li-ion
Cout:33uF(electrolytic cap)×2,22uF(ceramic)×1
Cin:22uF(ceramic)×2,0.1uF(ceramic)×1
L:8.2uH
HsideFET:TPN8R903NL
LsideFET:TPN2R703NL(Gate‐GND:1000pF)
RBTST:3.3Ω

Best regards,
Yusuke