This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24075: bq24075

Part Number: BQ24075

EN1 -0V ,EN2 -5V,TS - 0.6V,-ILIM 1K i had only 1K instead of 1.1K in my stock, R-ISET 866 ohm,\

I wanted to charge my battery at 1A because i am using 2500mah,3.7V and i want to charge my battery in 2.5 hrs only.

Input is supplied from DC power supply Input voltage :5V

My problem is current consumed from DC power supply is never exceeding 0.2A,With this current battery took almost 6 hrs.  to charge from 3V to 3.8V(which is not even full capacity of battery).How to set the fast charge current to 1A, So that my battery will charge in 2.5A considering no Efficiency loss.

Thanks & regards,

P.Akhil