Hi team,
TPS6590378 user's guide shows OFF2ACT Sequences and ACT2OFF Sequences in 6.1 and 6.2.
How long is delay from On Request to SMPS8, also from Off Request to RESET_OUT?
Best regards,
Hideki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
TPS6590378 user's guide shows OFF2ACT Sequences and ACT2OFF Sequences in 6.1 and 6.2.
How long is delay from On Request to SMPS8, also from Off Request to RESET_OUT?
Best regards,
Hideki
Hi Hideki,
I have assigned your post to our device expert. Please excuse a delay due to the holidays. Our expert will get back to you as soon as they can.
Thanks,
Gerard
Hello,
I will answer this thread later today.
Regards
Hello Hideki,
I could not find the paragraphs you mentioned in the user's guide. Would you please send the link for this document?
Regards
Hello Mahmoud,
The title is TPS659037 user's guide to power AM574x, AM572x, and AM571x (Rev. F) in product folder.
Can you open the below link?

Regards,
Hideki
Here is the delay for ON request. It is in the datasheet SLIS165G
ON Requests
ON requests are used to switch on the TPS659037 device, which transitions the device from the OFF to
the ACTIVE state. Table 5-9 lists the ON requests.
Table 5-9. ON Requests
EVENT MASKABLE POLARITY COMMENT DEBOUNCE
RPWRON (pin) No Low Level sensitive 16 ms ± 1 ms
PWRON (pin) No Low Level sensitive N/A
Part of interrupts
(event)
Yes (INTx_MASK register.
Default: Masked) Event Edge sensitive N/A
POWERHOLD (pin) No High Level sensitive 3 - 5 ms typical
Regards
Hi Mahmoud,
I understand a little around the event occurring, but what does debounce mean in this paragraph?
In addition, is there no regulation for N/A?
Regards,
Hideki
Hello Hideki,
I guess we can simply say it is a delay. During this delay an event (due to noise for example) is not considered. N/A means no debounce time. I hope this answers your question.
Regards