This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z80: best generic ID for ROM based devices

Part Number: BQ40Z80
Other Parts Discussed in Thread: GPCCHEM, BQ27426,

Dear TI Team,

I used the gpcchem online tool to get the ChemID what matches best a six cells battery pack (Type: INR21700-40T).  It looks like it worked with the ID 2162. The Error is under 3%.

But what is the second part of the report telling me? (After: Selection of best generic ID for ROM based devices like bq274xx)

Does that mean, that this gauge does not support the ChemID or should I just program the recommended ID  2162?

It would be great if you could help me with this question!

Best regards,

Anna

Report:

Chemistry ID selection tool, rev=2.5        
        
Configuration used in present fit:        
ProcessingType=2        
NumCellSeries=6        
ElapsedTimeColumn=0        
VoltageColumn=1        
TemperatureColumn=2        
CurrentColumn=3        
        
Best chemical ID : 2162    Best chemical ID max. deviation, % : 2.42    
        
        
        
Summary of all IDs with max. DOD deviation below 3%        
        
Chem ID    max DOD error, %    Max R deviation, ratio
2162    2.42    1.26
2161    2.69    0.43
2646    2.69    0.84
2141    2.9    0.29
        
Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge.        
        
        
Selection of best generic ID for ROM based devices like bq274xx        
        
        
Device / Family #1        
Generic Chem ID    Device/ Voltage/ Chemistry    max DOD error, %
3142    bq27421-G1D: 4.4V LiCoO2    21.2
354    bq27411-G1C: 4.35V LiCoO2    23.4
128    bq27421-G1A: 4.2V LiCoO2    24.43
312    bq27421-G1B: 4.3V LiCoO2    29.35
Best generic ID 3142        
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule        
        
        
Device / Family #2        
Generic Chem ID    Device/ Voltage/ Chemistry    max DOD error, %
1210    bq27621:  (ALT_CHEM1) 4.3V LiCoO2    21.94
1202    bq27621: (default) 4.2V LiCoO2    22.34
354    bq27621:  (ALT_CHEM2) 4.35V LiCoO2    23.4
Best generic ID 1210        
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule        
        
        
Device / Family #3        
Generic Chem ID    Device/ Voltage/ Chemistry    max DOD error, %
3142    bq27426: (ALT-CHEM2) 4.4V LiCoO2    21.2
1202    bq27426: (ALT_CHEM1) 4.2V LiCoO2    22.34
3230    bq27426: (default) 4.35V LiCoO2    25.21
Best generic ID 3142        
Warning: Generic ID Deviation is so high that it is most likely due to anomaly in the data. Please check that data files have recomended format, units and test schedule