This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: Gauging Parameter Calculation not successful

Part Number: BQ34110

Hello, I've tried multiple times and no success. Zip file is attached. The battery that I'm testing is Tenergy LiFePO4.

12.8V nominal, 9.9Ah, 13.8V charge voltage, 4A max discharge.

What am I doing incorrectly?

I have tried it with the files having header row and not having header row, it didn't work either way

Thanks,

Derek

Xology20201222B_without_header_row.zip

Xology20201222A.zip