Part Number: BQ40Z50-R3-DEVICE-FW
Hi
BQ40Z50-R3 set the register as below:
GPIO_EN, turn off LED_EN.
Settings-Configuration:
Flag Map Set Up is set to 0x8434 to pull GPIO LEDCNTLA (Pin20 pin) high when the Charging Status is in HV state.
Flag Map Set Up set to 0x8234 can pull GPIO LEDCNTLB (Pin21 pin) high when Charging Status is in HV state.
Flag Map Set Up is set to 0x8634, but GPIO LEDCNTLC (Pin22 pin) can not be pulled up, and also can not pull up by writing 0x0040 using GPIO Write().
How the set this register?
Thanks
Star