The current limit of TP16630 is 0.6A to 6.0A (± 7%). I would like to change this device to a pin compatible product of about 10A. Is there a device that can be replaced?
VIN is used at 24V.
The package is VQFN (24).
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The current limit of TP16630 is 0.6A to 6.0A (± 7%). I would like to change this device to a pin compatible product of about 10A. Is there a device that can be replaced?
VIN is used at 24V.
The package is VQFN (24).
Hi Yachi,
We don't have 10A part in same package. You can use two TPS16630 in parallel for higher currents.
Please refer https://e2e.ti.com/support/power-management/f/196/p/955040/3530866#3530866 for more details
Best Regards, Rakesh
HELLO Rakesh
thank you for your answer.
I have an additional question.
1. Please tell me the precautions when parallelizing
Example) Make the ILIM value the same, etc.
Hi Yachi,
1A) ILIM should be separate as per the device architecture to avoid disturbance with the current limit control loop
2A) Considering tolerances, we suggest to treat 11.1A as safe max load to support in 12A current limit configuration.
Best Regards, Rakesh