Hello TI,
As per the observation, when we are using different input adaptor for testing which 5V and different current rating input adapter,
1st adaptor which is 5V/3A
2nd adaptor which is 5V/5A
Observation is,
1. 1st adaptor which is 5V/3A ,
Input voltage - 5V
Input current - 3A
Bq24773 output voltage - 3.49V (No load)
Vregn voltage - 4.74V
Note - at first run Bq24773 output voltage - 4.4V (No load) but after some time Bq24773 output voltage get change which is 3.49V, now continuously show's Bq24773 output voltage - 3.49V.
Observe results are on Default configuration and battery is not present.
2. 2nd adaptor which is 5V/5A
Input voltage - 5V
Input current - 5A
Bq24773 output voltage - 4.4V (No load)
Vregn voltage - 4.74V
Note - Observe results are on Default configuration and battery is not present .
Notice this issues at also on different board, there is no any board issues
How to resolve this problem and what is the root-cause of the issues ..?
Thank,
Rahul